3/11/2024 8:42 PM | |
Joined: 1/5/2016 Last visit: 4/26/2024 Posts: 6 Rating: (0) |
Hi, thank you very much for all your posts, they were very helpful. Rigth now I´m working with Parameter Sets on TIA V19 and I´m facing a big problem. I want to handle Parameter Sets without using the ParamterSet Control and for that I´m trying to use Edit Tag property of the Parameter Set Type. The problem is that the PLCUDT that I´m using in the Parameter Set Type has other PLCUDT inside (This help me to have better data structure and better data handling in the PLC) but I can´t create a HMIUDT with the same structure than the PLCUDT. This is very disappointing because the only solution I have thougth is that I´m gonna have to create a very simple PLCUDT with a bounch of data and this will make me have to handle data in a more complex way. I think the use of UDT´s in Parameter Sets has a very big potencial and eficiency, but this this problem is a step backwards of using UDT´s for Parameter Sets. Do you have any suggestion?
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/12/2024 14:54:07New subject after splitting |
|
Follow us on