3/13/2024 6:24 AM | |
Joined: 3/30/2020 Last visit: 4/28/2024 Posts: 4459 Rating: (931) |
It sounds as if you are already following the directive given in the article.. Did you make 100% sure that you loaded the hardware configuration? The PLC name should be highlighted when doing a download. Some people confess on the forum to have only downloaded the software part. As a sanity test make a new small project. Set the CPU firmware as V2.8 in the hardware configuration, but leave the actual loaded firmware as is. Have the minimum functionality to test the link of CPU and HMI. Do you still have problems? Follow up by updating the firmware in the hardware configuration to match the V2.9 firmware in the device. Test again. If you still are faced with problems, consider using the "Support Request" link to also chat with Siemens. Please do let us know on the users' forum what your findings are. Good luck. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on