3/19/2024 2:07 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, You can use one of the standard blocks. I don't know exactly what you mean with PCS v3 library, but there are two versions: classic or APL. I assume it is APL. You can use a MonDiL or MonDiS block to create alarms. Via the properties of the block, you can click on a button: Messages where you can define the message class, name of the message and other properties like acknowledgment. You also use another block like EventTS or Alarm8P to create alarms/messages. |
If I could help you, you can use the RATE button. Thank you. |
|
3/20/2024 7:25 AM | |
Joined: 1/25/2024 Last visit: 4/3/2024 Posts: 4 Rating: (0) |
Thank you, that's what I've been looking for |
Follow us on