11/19/2021 7:14 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi Plceler, do you mean this application sample? Connecting a S7-1200 / S7-1500 to a SQL DatabaseI´m afraid no. You could try to change any usage of the command string inside the block and also thier following instructions, like Strg_to_Char to WStrg_to_WChar and the Array of Bytes to an Array of Words. It could work. If it works, don´t forget to tell us. regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
11/2/2023 11:51 AM | |
Joined: 4/25/2017 Last visit: 4/4/2024 Posts: 424 Rating: (65) |
Hey, If you would have searched a bit longer you would have found it: Forum: Added support for longer SQL queries for S7-1500 and SQL DB |
Best Regards, |
|
Follow us on