3/26/2024 10:30 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, You can use the GrpErr to detect a problem with the MonDiL. A CSF error will be generated by the driver block connected-> From driver.Bad to MonDiL.CSF You can also use the Signal Status of PV_Out to check the status of the input signal. 16#00 means Bad signal device related. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on