4/4/2024 6:36 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating: (0) |
When try to create a new project, we go to Insert>station and there is no ET 200SP on the list. We tried to update hardware catalog from HERE but to no avail. Do we need to use "other station" in order to create a project for the ET 200SP? Or there is some other way? We have step7 V5.7 on Windows 10. Do we need to install an older version for ET200SP to show up? |
Last edited by: Jen_Moderator at: 04/04/2024 12:05:34Link optimized. |
|
4/4/2024 7:31 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating: (0) |
it's a CPU i think |
4/4/2024 7:41 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981) |
yes this is a cpu and can only programmed with TIA POrtal not with the classic Step7 V5.x |
4/4/2024 7:50 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating: (0) |
thanks! |
Follow us on