4/12/2024 7:19 AM | |
Joined: 5/6/2023 Last visit: 9/20/2024 Posts: 10 Rating: (0) |
How can I access User Administration in Runtime is activated in Unified MTP700 Comfort. There used to be a user view function in TP Comfort Panel where we can add, delete and assign group to user in runtime. Is this function removed in Unified HMI panels....? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/12/2024 10:01:01New subject after splitting |
|
4/12/2024 10:37 AM | |
Joined: 5/30/2022 Last visit: 9/24/2024 Posts: 582 Rating: (96) |
Hi AutoGen_1597649, The available options are as follows: Options for local user management My recommendation is to add a Web Browser in the panel project and enter the following web address: https:// IP /UMC |
If this information really helps, you could use the Rate function. |
|
4/15/2024 7:24 AM | |
Joined: 5/6/2023 Last visit: 9/20/2024 Posts: 10 Rating: (0) |
Hazard_7 thanks for reply. It is showing error. I have attached image of error. |
Follow us on