1/9/2024 8:20 AM | |
Joined: 12/7/2023 Last visit: 6/25/2024 Posts: 5 Rating:
|
Little up ;) |
1/9/2024 2:39 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating:
|
Have you configured and located the SIMOCODE devices behind a Y-Link or just single sided on one of the controllers? Are you using any of the SIMOCODE PCS7 libraries or a custom integration? |
If my post helped you, please rate. Thanks. |
|
4/23/2024 10:29 AM | |
Joined: 12/7/2023 Last visit: 6/25/2024 Posts: 5 Rating:
|
Behind an Y-link with the library from siemens. No customisation |
4/23/2024 3:31 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating:
|
There are 3 supported compatible libraries for PCS7 9.0 SP2. Which one are you using since you didn't answer? SIMOCODE pro PCS 7 Library v 9.0 SP2 < most likely one you are using if its a new plant If you are not using one of those specific versions you have to do that first. Now as to your specific problem, some part of what you are saying doesn't make sense. If you perform HW download in RUN does everything work fine? With H-system you should be able to make nearly all your changes in RUN, even whatever you mean 'make connections' if that's NetPro just download selected info, not the whole station so no STOP. |
If my post helped you, please rate. Thanks. |
|
Follow us on