4/11/2024 9:20 AM | |
Joined: 5/29/2013 Last visit: 5/15/2024 Posts: 27 Rating: (0) |
Good day, first of all just for information, I did use pn/pn couplers (6ES7158-3AD10-0XA0 ) before in the projects and had no issues to set them up. this one is a bit special I guess, thats why I am here I have two s7-1200 plcs in different networks, pnpn coupler is between them. X1 and X2 sides have unique pn-name and unique IP in each network X1 and X2 are mirrored (IN-OUT, OUT-IN) X1 and X2 are visible online in the list, online diagnostics is visible or both all diagnostics bits are unchecked already X1 looks fine in the project (green, no faults) X2 looks bad like it is not configured at all or configuration is wrong. The problem is seen not only with the submodules, but also with the main module in hw configuration tree online. I did try fw 3 IO modules, I did power off PLC, pnpn coupler, checked cables, reset modules and configured again and again. Have a very strange feeling, that X2 side does not take in the configuration.... Is it possible?? AttachmentPNPN coupler issue.pdf (10 Downloads) |
Follow us on