5/13/2024 7:32 AM | |
Joined: 9/30/2016 Last visit: 6/12/2024 Posts: 913 Rating: (6) |
Please also see the attached screenshots. I have to alarms that are supposed to work in the same way (and have done so previously). Now the left alarm is only working partially - it sets the alarm bit that the HMI reads so it does generate an alarmline in the HMI but it does NOT set the alarm bit that the PLC uses to stop an action and trigger both audible and visual alarm (like the right one does. I hope you can help me with 2 things: 2) Can you please translate the STL code from Network 78 to ladder code for me?
AttachmentBumperbars.zip (34 Downloads) |
Follow us on