5/25/2024 4:42 PM | |
Joined: 6/6/2017 Last visit: 6/17/2024 Posts: 44 Rating: (0) |
Good morning everyone! I am having a very specific problem with my S7 Simatic Manager. I bought a new computer (Asus ZenBook Duo) that is equipped with the new Intel Meteor Lake architecture (Intel Core Ultra 9 185H). Basically, I was able to install all the software that I normally use, however, the S7 Simatic Manager (V5.7 + SP1) loses the connection interfaces when I try to open a compared block. The strange thing is that I can monitor logics (without doing the comparison) before trying to open a block that I compared. Sorry for the difficult explanation, it's really a very specific problem. Trying to summarize with a timeline: 1- Open the Set PG/PC interface: OK Thank you in advance. AttachmentSiemens Problem.zip (9 Downloads) |
Follow us on