2/2/2021 5:25 AM | |
Posts: 2 Rating: (0) |
Hi, I need help regarding the connection of IOT2000 to the internet. Ive already connected my X2 port to the router and X1 port to my pc for putty. I cant access to the internet to install node-red to the iot2000. I have followed several guidelines from the forum but I still got ping: bad address 'google.com' when I tried to ping google. Please help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/02/2021 12:37:31New subject after splitting |
|
2/4/2021 12:47 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (378)
|
Hi, usually setting the interface to dhcp and connect it to a dhcp router (connected to the internet) is managing everything for you. Now you set a static IP address. I guess your routers IP address is 192.168.0.1? I'd remove the line "network 192.168.0.0". Did you restart the IOT after changing the /etc/network/interfaces file? Because simply changing the file does not update the interfaces, this only happens when the interfaces or the whole IOT is restarted. Using a static IP requires some more to dos for the nameserver: You need to remove the link of /etc/resolv.conf, re-create the file and enter your routers IP address and Googles DNS and make the file immutable afterwards. For a detailed description with the commands see here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on