3/22/2017 6:35 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi Eli_47, Can u share the manual u r referring. As per manuals with me(V5.5), H_CTRL is used to influence update, linkup modes and self test disabling. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
3/22/2017 9:19 PM | |
Joined: 8/23/2012 Last visit: 8/20/2024 Posts: 118 Rating: (4) |
Sure, it is from step 7 help AttachmentControlling Operation in H Systems with SFC 90 _H_CTRL__.pdf (607 Downloads) |
3/23/2017 5:23 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi Eli_47, Thanks for manual. As per manual, u should be able to switchover master/standby with mode decimal 30, 31 or 5. Probably latest version of SFC or higher CPU like 414 or 417H could resolve problem. Not sure!!! |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
3/23/2017 9:02 PM | |
Joined: 8/23/2012 Last visit: 8/20/2024 Posts: 118 Rating: (4) |
Lattest version of SFC... you mean i need to update firmware? |
Follow us on