6/23/2009 8:56 AM | |
Posts: 53 Rating: (2) |
Hi, sorry forgot about program. Here is. Henio. AttachmentOfukovace.zip (263 Downloads) |
6/23/2009 5:15 PM | |
Posts: 191 Rating: (58) |
Hi!! i made this project and at least it is compiling... it does shows errors if i compile it without an input or an output, but if i fill all of them it compiles... ¿¿ is this what you are trying to do ?? ROSA Attachmentxxx.zip (251 Downloads) |
6/24/2009 7:16 AM | |
Posts: 217 Rating: (52) |
Hello, I also agree with Rosa. I also check your program and call your subroutine but it seems to be OK. Best regards. |
6/24/2009 9:40 PM | |
Posts: 191 Rating: (58) |
Hi!! ¿¿ could you compile the "empty" project iposted ?? ROSA |
6/25/2009 8:40 AM | |
Posts: 53 Rating: (2) |
Hello, no, i cannot. But when i add a INPUT variable (nonBOOL) ro your subroujtine, then i can :) Henio. |
Follow us on