7/26/2024 11:01 AM | |
Joined: 5/8/2019 Last visit: 7/31/2024 Posts: 1 Rating: (0) |
Hi I am not sure if this is the right place to make a query on Continuous Power Consumption of the elements of the PAC1200 Current Monitoring System to monitor the currents in a large number of circuits in a MCB Distribution Board. Hope someone can help me. I find that the 7KTPAC1200 is a low cost current monitoring system and wish to consider using it LV Power Distribution Boards. The basic elements 7KY1260 and the 7KT12xx series Sensor Bars would always be powered. Hence I am interested in computation of Energy consumption of these elements. Can someone please help with the data of power consumption in VA and Watts of: 7KT1260 and sensor bars 7KT1242 (for 12 CTs), 7KT1238 (for 9 CTs), 7KT1236 (for 6 CTs), and 7KT1233 (for 13CTs). Thanks GGRU ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 07/29/2024 12:31:04New subject after splitting |
|
Follow us on