4/2/2024 4:09 AM | |
Joined: 9/5/2019 Last visit: 4/1/2024 Posts: 8 Rating:
|
I have another project to start working on on my Mac however my Mac says that the version I have now doesn't work (presumably after Sonoma update) Is there a new version of LOGO Soft Comfort for mac. If so where do I get it from? Thanks Mark ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/02/2024 04:10:09New subject after splitting |
|
4/2/2024 4:22 AM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33656 Rating:
|
There's no special upgrade only for MAC. The current LSC version is V8.4. You can download the upgrade from here: Download and installation instructions for LOGO! Soft Comfort Upgrade V8.4 |
4/2/2024 5:07 AM | |
Joined: 3/30/2020 Last visit: 8/30/2024 Posts: 4708 Rating:
|
Have a look at your Java Runtime Engine. That may be the piece that needs upgrading. Regular volunteers are PC users. It may take a while before a fellow Mac user comes along. Consider contacting Siemens by using the "Support Request" link. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
8/11/2024 3:37 PM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33656 Rating:
|
Siemens has not tested LSC V8.3 with your OS. |
Follow us on