8/2/2024 12:03 PM | |
Joined: 7/11/2024 Last visit: 9/6/2024 Posts: 38 Rating: (3) |
Hi vlade200 Does it also happen if you create a test project?In that case, it seems that the WinCC installation is corrupted and it would be interesting to reinstall it again. I understand that when you say that you reset the PC you mean to restart it. If it only happens with that project in question I would try, first, to delete the DCF as you can check here: Update configuration file of the WinCC project (delete DCF) Good luck! |
If this comment was helpful, be sure to rate it! |
|
Follow us on