8/21/2024 12:03 PM | |
Joined: 7/29/2024 Last visit: 8/21/2024 Posts: 2 Rating: (0) |
I have a Problem with aktiv Homing using Tia Portal. I have done all necessary configuration on technologie Object. When i press the home Button, the motor runs with the approach Velocity of homing, then i press the referenz Button and the motor continous to move but this time with the referenz Velocity. Everything seems to be okay still yet. I actually expect the motor to run and stop after sometimes (When arriving at the home Position, wich i set at value zero). But the motor doenst and just keep mooving without stopping passing the zero Position and going in the negative direction. When i one more time press the Referenz Button, the motor actually stops and set the actual Value as Home Value (Position Zero). Can Someone please explain to me why, i actually have to press the ReferenzButton two times instead of one time to home my axis ? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/21/2024 12:05:58New subject after splitting |
|
8/21/2024 12:07 PM | |
Joined: 7/30/2024 Last visit: 11/8/2024 Posts: 319 Rating: (7) |
Closed because posted twice. The active topic can be found here:
Kind regards, Moderator_Lan |
Follow us on