8/28/2024 8:33 AM | |
Joined: 8/16/2018 Last visit: 11/5/2024 Posts: 4 Rating: (0) |
My client has supplied me with an old Siemens data sheet that describes an Analogue 2oo3 Selector block. I think the data sheet is 20 years old, and I have not come across this block in previous projects using APL. Does anybody know if this block was ever updated or what library it might have originally appeared in? Or could suggest equivalent block that could be used in a PCS7 v10 project? AttachmentSiemens Standard ASEL3 Function Block.pdf (169 Downloads) |
8/28/2024 10:15 AM | |
Joined: 3/14/2008 Last visit: 11/5/2024 Posts: 2122 Rating: (950)
|
Hi, Please find enclosed the link for the manual of the Industry Library. This is an addon library for PCS7 and in the library is a block called VoteAnL (page 644). I think this is the block you need to replace ASEL3. ASEL3 is not known to me, it's not a supported block anymore. |
Last edited by: Oreca at: 08/28/2024 16:16:43Added the link If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
8/28/2024 11:54 AM | |
Joined: 8/16/2018 Last visit: 11/5/2024 Posts: 4 Rating: (0) |
Thanks, the VoteAnL block is exactly what I need :) |
Follow us on