9/5/2024 9:37 AM | |
Joined: 3/11/2019 Last visit: 10/14/2024 Posts: 1597 Rating: (291) |
Hi, as you already asked, yes it is possible simply to put the old SMC into the new CPU. So you do not need to download the project at all. Maybe the new CPU will also be recognized correctly afterwars. If the SMC is not availalable anymore, you can also transfer the program directly to an SMC via TIA and use the SMC afterwards. So you will not have any troubles with establishing an online connection. Download project data into the S7-1200/S7-1500 CPU without TIA Portal-> Option 1: Download configuration directly to the memory card. regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on