6/17/2024 7:22 AM | |
Joined: 4/20/2020 Last visit: 6/20/2024 Posts: 4 Rating: (0) |
Hello, i have a new VMWare virtual machine with Windows 10 Enterprise 22H2. I have installed: - S7 V5.7 - Tiaportal V14 Update 10 - Tiaportal V15 - Tiaportal V15.1 Update 8 - Tiaportal V16 Update 6 - Tiaportal V19 Update 2 Tia administrator V3 At tthe moment i use the version V15 and V16. Initially both versions crashed when I try to go online. I solved it by removing a Windows update: https://support.industry.siemens.com/cs/us/en/view/109971630 Now the tiaportal crash when i close the project or the application with this error: System.IO.FileNotFoundException: Could not load file or assembly 'S7O.CommonInterfaces, Version=901.300.105.3, Culture=neutral, PublicKeyToken=null' or one of its dependencies. The system cannot find the file specified. Can you help me? |
Last edited by: The Helping Hand at: 06/17/2024 10:19:45Link optimized |
|
9/30/2024 3:42 PM | |
Joined: 1/8/2018 Last visit: 10/29/2024 Posts: 3 Rating: (1) |
Hello, were you able to resolve this issue? I am facing the same problem. Many thanks. |
10/1/2024 2:24 PM | |
Joined: 1/8/2018 Last visit: 10/29/2024 Posts: 3 Rating: (1) |
Here is the solution: https://support.industry.siemens.com/cs/es/en/view/109972630 |
Last edited by: Moderator_Lan at: 10/01/2024 14:25:40link optimized |
|
This contribution was helpful to2 thankful Users |
Follow us on