10/3/2024 8:21 AM | |
Joined: 11/12/2008 Last visit: 11/8/2024 Posts: 205 Rating: (16) |
Hello, Here I tried , to popup MsgBox in WinCC Flexible it's work and may it will Help. 1- Open Notepad application. 2- Write the message as in attached and the message Should be Exclamination to be Top of most. 3- After writing the message, save the file as (FileName.vbs) in vbs format. 4- Open WinCC Flexible and write the attached script. (StartProgram"YOUR FILE COMPLETE BATH WITH FILE EXTENTION", "", hmiShowNormal,hmiNo 5- Asign the script to Button event or to input Regards AttachmentPictures.zip (79 Downloads) |
Last edited by: H.SAPER at: 10/10/2024 05:34:45HASSAN.S POJAILA |
|
Follow us on