5/5/2022 11:21 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, on the IOT2050 Advanced with FS:02 the Industrial OS is pre-installed. The device boots from the internal eMMc with Industrial OS automatically, the SD card is not considered by default. For more information please see here. An overview about the different FS can be found here. Btw: How do you know the firmware when you don't have access? Or are you using a UART cable? In this case you can change the boot order without following the whole installation process of IndOS. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
5/5/2022 12:36 PM | |
Joined: 5/3/2022 Last visit: 4/2/2024 Posts: 12 Rating: (0) |
Can we Start on Step " Use of the UART cable " For Boot the device Right ? Best regards!
|
10/4/2024 8:47 AM | |
Joined: 7/30/2024 Last visit: 10/4/2024 Posts: 176 Rating: (3) |
New question published by AutoGen_6442597 is split to a separate thread with the subject can't ping the IOT with adress 192.168.200.1. Best regards |
Follow us on