3/19/2025 3:49 PM | |
Joined: 2/7/2025 Last visit: 3/28/2025 Posts: 1 Rating:
|
Hi. I have the same problem, but when I insert SinaParaS it did not communicate with the driver (Error 1) . It is so strange because the telegram 111 is communicating 100% because I can move the servo. In the screenshot I was trying to read the parameter 2585 and it should show me -300 but did not work. I also put an screenshot from the sinapos to show that the telegram is working. I can't use the Startdrive, I'm just using the starter software and tia portal v18. I'm using an s7-1200 and CU310-2PN with a PM240-2. Thanks. ------------------------------------------------------------------------------------------ Attachmenttia portal.zip (170 Downloads) |
Last edited by: Moderator_Lan at: 03/19/2025 16:17:12New subject after splitting |
|
Follow us on