3/6/2025 3:48 PM | |
Joined: 12/10/2024 Last visit: 9/4/2025 Posts: 1 Rating:
|
Hi, In a project of mine, I need to separate an existing S7-400H system in two different cabinets. At the moment, both PLC are located in the same cabinet. The two cabinets are located far one from another (>10m), hence I did plan to use sync module 6ES7960-1AB06-0XA0. However, these cabinets are connected by existing multimode FO and we did not plan to install monomode FO. If I use a switch equiped with the adequate SFP in order to convert FO signals, will the redundancy still work ? You'll find attached a drawing of what I want to achieve. Many thanks AttachmentFO Diagram.pdf (420 Downloads) |
Follow us on