(0)| 4/14/2025 7:43 PM | |
|
Joined: 1/4/2013 Last visit: 12/20/2025 Posts: 1195 Rating:
|
Sorry for the strong title, but I really lost one working day because of this and still no solution. TIA20 (also tried with TIA20 Upd1) Comfort Panel KP 900 PLC 1215DC/DC/DC PLC part is perfect. When I insert the HMI and I declare one page without nothing, it compiles. Whenever I declare an IO field, and after that I point to a PLC variable (which is a trivial operation of course, that I did thousands of times), if I try to compile (or rebuild all, same result), I see the infamous error "Contact Siemens Support". If I delete that IO field, compile is ok, but HMI is useless of course. If I close TIA portal I get a non critical diagnostic exception (which is attached), but it comes only when I close TIA What I have tried : 1) Do a repair of TIA portal using its original installation program Everything gave the same identical result : Contact Siemens Customer Support. Super important note : when I use a Basic Panel, no issues happens, everything is PERFECT. Danke guys Attachment66a0f6d0-5e9f-46f7-a8e6-53293bd439e2.zip (259 Downloads) |
Last edited by: Davinator at: 04/14/2025 20:12:04Searching for Siemens used/new equipments ? |
|
Follow us on