4/16/2025 7:03 AM | |
Joined: 4/16/2025 Last visit: 4/21/2025 Posts: 2 Rating:
|
Hi I'm new here and also new at my job. I hope you understand my terms. I was having a problem identifying on what is being faulty in our current set-up. By the way this system is functional until we noticed that the process monitoring in Operator Stations and HMI are not anymore available/no data. In this particular AI module we are using all 8 channels from 0-7, 5 channels are found to be not functioning properly. Channel 0 is a level sensor, Channel 4,5,6,7 are pressure sensors For now here is my as found conditions in both PLC side and sensor side. Injected 8mA to all 5 channels while temporarily disconnecting the sensors, and performed module monitoring for HEX values. Channel 0,4,5,6,7 - from W#16#8000 to W#16#1C3F. Channel 0 - data changes in HMI and Operator Stations (level monitoring changes or has data upon injecting a certain current signal. Channel 4,5,6,7 - No value in both HMI and OS. Upon checking module information's diagnostic buffer these events are active: 1. ADC/DAC error 2. Missing external voltage 3. Module without parameters and below that is ADC/DAC error Internal error, Incoming event. When all sensor are connected to the module Level sensor - no display but when I tried to power it using a field communicator the sensor's status is okay and display in the sensor is available. Pressure sensors - All pressure sensors have display but no data in HMI/OS. And also I tried to replace the AI module but same problem is encountered. I have attached captured images for reference. Thanks :D AttachmentDoc2.docx (293 Downloads) |
Last edited by: dr!lRDD2066 at: 04/16/2025 07:24:09 |
|
4/16/2025 7:10 AM | |
Joined: 4/16/2025 Last visit: 4/21/2025 Posts: 2 Rating:
|
I've added the video during the time I was injecting 8mA to the 5 channels.
Attachment491530673_9545201498925810_2784495501421675924_n.mov (313 Downloads) |
Follow us on