(0)| 4/23/2025 2:43 PM | |
|
Joined: 4/23/2025 Last visit: 7/15/2025 Posts: 2 Rating:
|
We are currently using an IOT2050 with firmware version V01.03.01 and the sample image v1.3.1.
We are usingNetworkManagerand managing the interfaces using In summary:P1 (LAN) is working, but P2 (WAN) is not. We kindly request support in identifying the cause and resolving this issue. AttachmentCaptura de tela de 2025-04-22 16-.zip (322 Downloads) |
| 7/15/2025 1:24 PM | |
|
Joined: 4/23/2025 Last visit: 7/15/2025 Posts: 2 Rating:
|
Hello, I have noticed that there are other topics reporting similar issues. Device:Siemens IoT2050
Behavior SummaryExpected BehaviorWhen the IoT2050 is powered on with port X2 connected to a network with an active DHCP server, it should receive and configure a valid IP address from the available pool. Actual Behavior
Alternative Procedure That Works
Steps to Reproduce the Issue
Possible Technical Cause
Supporting MaterialA video was recorded demonstrating:
Attachment2025-06-30_15-49-08.zip (181 Downloads) |
Last edited by: Moderator_Lan at: 07/15/2025 14:21:48File attached from link. |
|
Follow us on