9/16/2025 6:57 AM | |
Joined: 8/15/2025 Last visit: 9/18/2025 Posts: 7 Rating:
|
Just a quick question. I have loaded PCS7 V9.0 successfully apparently… but I am trying to run this installation on a VM as I don't normally use windows operating systems. The Host operating system is Ubuntu 22.04.5LTS and the guest operating system is Windows 7 Ultimate. I was hoping to be able to run the Windows7 Ultimate guest operating with the PCS7 V9.0 installed, then follow the PCS7 V9.0 Getting started project manual part 1…. I hoped to run the Simatic PLCSIM as I have no Hardware obviously. I have many screenshots of the PCS7 V9.0 installation from DVD1 and DVD2, with licensing. Installed packages as such to confirm the current installation if the idea of running such a setup is at all possible. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/16/2025 07:29:36New subject after splitting Colin Canham |
|
9/17/2025 7:10 PM | |
Joined: 12/22/2021 Last visit: 9/17/2025 Posts: 61 Rating:
|
hello Windows preparation
VM configuration
|
Follow us on