10/6/2025 5:27 AM | |
Joined: 1/21/2013 Last visit: 10/6/2025 Posts: 4146 Rating:
|
Hi, TIA Portal's diagnostics are primarily used for PROFINET devices because they can receive PROFINET-specific diagnostic data. While you can view some general device information in the diagnostics view for other network devices, the Web Based Management (WBM) tool is probably used for configuring and diagnosing industrial routers like your SCALANCE M876-4. Unfortunately, I'm not sure what you saw or expected to see in the diagnostics view today. However, the deviation is most likely not an issue with the TIA Portal or the used firmware version. While you can download an older firmware version, it is not recommended since those versions are end-of-life products. You can load the firmware using WBM. Kind regards |
This contribution was helpful to
2 thankful Users |
Follow us on