(0)| 10/16/2025 4:21 AM | |
|
Joined: 1/28/2016 Last visit: 11/4/2025 Posts: 462 Rating:
|
Hi, I use WinAC in vmware, also withe the “bios440.filename="FUJITSU211_314.ROM". It worked fine in vmware 17.6.3 under Windows 10. Since 2 weeks I have Windows 11, also vmware 17.6.3, and my VM with WinAC boots with a black screen. When I remove the line with the ROM in the vmx file, the VM boots, but I can't open WinAC. Is there some known issue with the FujitsuROM under Win11? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/16/2025 10:39:59New subject after splitting If this Information really helps, you could use the Rate function |
|
Follow us on