(0)| 10/26/2025 2:02 PM | |
|
Joined: 12/19/2019 Last visit: 12/12/2025 Posts: 488 Rating:
|
Here you have two options to choose from. It would be interesting to know which version you prefer. Regards, Quirin AttachmentOFF AUTO MANUAL.zip (30 Downloads) |
This contribution was helpful to
|
|
| 10/26/2025 4:29 PM | |
|
Joined: 6/11/2019 Last visit: 12/14/2025 Posts: 2702 Rating:
|
Hello Qurin, Your suggestions are well-intentioned, but if a wire breaks at the switch during operation, you won't be able to shut it down. I've also thought of something that takes wire-break safety into account and shuts down the system in the event of an interruption. But I personally consider this a very poor solution, too, since the operator may not be immediately aware of the switching mode, and the system will start up with a delay after the time set in B005 has elapsed. This could lead to misinterpretations or even accidents. Regards Ella_68 AttachmentProgrammplan-Auto-Manual.zip (26 Downloads) |
This contribution was helpful to
|
|
| 10/28/2025 4:01 PM | |
|
Joined: 7/31/2021 Last visit: 10/30/2025 Posts: 11 Rating:
|
Hello Quirin , Ella Thanks for the support Here included the program (watch C up) Via my mobile phone I can set the heating off/ auto or manual. There is just one small thing , is there a way so I can view the state of the heating in one text line. Now the line moves around because of the three states of the relay's. It's just a minor issue Kind regards AttachmentOude heibaan 35 versie 2.1.zip (30 Downloads) |
| 10/29/2025 6:13 PM | |
|
Joined: 10/17/2018 Last visit: 12/11/2025 Posts: 58 Rating:
|
Greetings. I hope this is helpful.
AttachmentOFF AUTO MANUAL as sequence_V.2.zip (34 Downloads) |
This contribution was helpful to
|
|
Follow us on