(0)| 11/21/2025 1:02 PM | |
|
Joined: 1/22/2025 Last visit: 11/21/2025 Posts: 7 Rating:
|
Hello, I have two logos connected to a CIM logo. One, 192.168.0.81, has an M1 mark in its programming that must be activated to send an SMS. The other logo, 192.168.0.82, also uses the M2 and M3 marks to send SMS messages. The logo with the IP ending in 81 works perfectly for sending text messages. However, the logo ending in 82, which uses the M1 mark, does not communicate with the CIM, but if I run the test on the CIM, the text message is sent. I have programmed the logo ending in 81 in the MB0 mark range (to use marks M2 and M3) and the logo ending in 82 in the MB2 range (to use mark M1). I filled in the data table in logo 8 (Logosoft version 8.4, logo selected in the Logosoft 8 programme FS4). In Ethernet connections (connection 1 (client S7 of 192.168.0.80, the IP of the CIM logo)), fill in the table as follows: local address MB 2, length 1, left direction, remote address MB2 length 1. In the CIM logo interface, in the data-variable management section, fill in the M1 mark with the address 2.0, but this way there is no communication between the Logo 8 and the CIM logo. Could you please help me? Thank you. Translated withDeepL.com(free version) |
| 11/21/2025 1:52 PM | |
|
Joined: 3/30/2020 Last visit: 11/21/2025 Posts: 5612 Rating:
|
< duplicate > See:There is no communication between logo 8 and the CIM |
Last edited by: qwazee at: 11/21/2025 13:54:20Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on