(0)| 11/18/2025 10:58 PM | |
|
Joined: 7/7/2010 Last visit: 11/21/2025 Posts: 16274 Rating:
|
Check this support site link for information for the s7-1200 and the s7-1500 for ISO-on-TCP communications and how to set them up. https://support.industry.siemens.com/cs/document/18909487 It is easier when both s7-1200 and s7-1500 projects are in the same TIA Portal project, especially when configuring the comm blocks. For example, from the above link, the PDF referenced for the s7-1500 provides configuration specifics to connect to an s7-1200 where it specifies the very hard to guess TSAD ID, starting on page 146:
Quite a lot of details are there but do require you to do a little work to locate it. I wish all those predefined values were automatically assigned as soon as ISO-on-TCP protocol were selected. Maybe in TIA Portal v30 they will be. |
|
science guy |
|
| 11/20/2025 1:29 AM | |
|
Joined: 9/10/2025 Last visit: 11/20/2025 Posts: 4 Rating:
|
Yes, I will be sending a screenshot of the connection parameters and the Documents to help understand the project. I’m working on a communication setup between two Siemens systems using ISO-on-TCP. The setup is based on the signal-exchange PDF included in the Google Drive link I shared. In this configuration, the cooling unit (my station — referred to as M2) must communicate with the mixer (M1). The goal is simple:
I have already created the communication DBs and written an SCL program for the S7-1214C (M2). Everything has been connected via Ethernet, but the two stations are still not communicating. I’ve uploaded my full project (including the SCL block and the communication PDF) in the provided Google Drive ZIP. If you could please take a look and point out what I may have configured incorrectly in the ISO-on-TCP setup or telegram handling, I would greatly appreciate your help. Thank you. |
| 11/20/2025 5:59 PM | |
|
Joined: 9/10/2025 Last visit: 11/20/2025 Posts: 4 Rating:
|
Hello, I’m working on an ISO-on-TCP communication setup between two Siemens systems. The project files, including my SCL program and the official signal-exchange PDF, are included in the Google Drive link I shared. In this setup, the cooling station (M2, my station) containstwo pump drivesthat must supply coolant when commanded. The mixer (M1) sends and receives the required signals. The communication requirements are: From M1 → M2 (Cooling station):
From M2 → M1 (Mixer):
I have created all communication DBs and an SCL block for the S7-1214C, and both PLCs are connected via Ethernet, but communication never establishes. If you could review the program and PDF in the ZIP file and help identify what I may have configured incorrectly in the ISO-on-TCP or telegram handling, I would greatly appreciate it. Thank you. AttachmentGREENFILED_COOLANT_14_11_25.zip (4 Downloads) |
Last edited by: samuel_rufus154 at: 11/20/2025 22:03:59 |
|
Follow us on