(0)| 11/25/2025 5:15 PM | |
|
Joined: 4/28/2015 Last visit: 12/5/2025 Posts: 3 Rating:
|
Thank you for looking into this. Attached are the photos you requested. Sorry. I forgot to include the most important detail... both POK and PR LEDs are steady green. All other LEDs are off. At no time do I see the CB LED flash amber. Yes, I do have Step7 Simatic Manager software. The PCMCIA card has been reloaded with NCU software (v07.04.32). History of NCUs Our system is strictly for machine simulation purposes. These components are not being used on machines. There are no drives or I/O connected to our system. Both NCU573.5’s were communicating recently (~3 weeks ago) when individually connected to the PCU50.3 in 1:1 (1 PCU + 1 NCU) configuration. When each NCU was communicating to the PCU50, they did have low battery alarms. The batteries have since been replaced. Voltage is 2.9 volts but is enough when it is used with our NCU573.4 that is communicating. When NCUs were connected together via the X101 connection for testing of an m:n configuration (1 PCU + 2 NCUs) is when communication problems appeared. At one point both NCUs X172 connections were also connected together and to the same U/E (I/R) module X351 connection for power source purposes. Could this have introduced problems in the NCUs? Also, at some point, we noticed one of pins one of the NCU’s X172 drive bus connector was bent such that it was not making contact with the ribbon cable connector. The second NCU may have been connected to the first NCU via the X101 connection at the time, however, I do not expect this to be source of our problem because pin was bent such that it was not shorting with the other pins. Bent pin is now corrected, changed back to 1:1 (1 PCU + 1 NCU) connection, restored original mmc.ini, deleted …oem\netnames.ini file, but cannot regain communication with either NCU. AttachmentOperatorPanelScreen_NCU_LEDs.docx (7 Downloads) |
Follow us on