(0)| 11/28/2025 2:33 PM | |
|
Joined: 7/4/2025 Last visit: 12/23/2025 Posts: 10 Rating:
|
Hello to all, i kindly ask support about manual installation on panel image in my TIAportal V18 Update3. I know that since Version 16 or 17 when TIA is installed on PC the panel image are not installed and need to install manually. I took from support SSIO Image-Downloads for SIMATIC HMI Operator Panels: Unified Comfort Panels - ID: 109825605 - Industry Support Siemens the file 109825605_Unified_Comfort_Panel_V18_0_Upd3.EXE. I've installed on the PC but i can not see in the help that WinCC panel image V18 is installed. Until now we are installing the panel image in the HMI by a tia V16, and after we make all the modify in TIA18 that we are using even for develop our PLC program. I ask support to avoid every time to use TiaV16 for download panel image on HMI ( comfort HMI) and after use V18 for work. Thnaks to all |
Last edited by: Moderator_Lan at: 12/01/2025 09:42:16Link optimized |
|
| 11/28/2025 3:05 PM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Hello, Perhaps you can give some information about the HMI Panel you have. If you have an Unified Comfort panel, you have downloaded the right file. But if you have a Comfort Panel, you must use the following link: Image Downloads for SIMATIC HMI Operator Panels: Comfort / Mobile / Basic Panels (Use the HMI_PIU_installer_2.0.0.0.exe) Best regards, Wizard |
Last edited by: Wizard at: 11/28/2025 15:05:54 |
|
| 12/23/2025 12:59 PM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Hello, Please go to the following link: Image Downloads for SIMATIC HMI Operator Panels: Comfort / Mobile / Basic Panels Because you have TIA Portal v18, you can use the "HMI_PIU_installer_2.0.0.0.exe" (See point 1.1) Or you can make an Offline install, see point 1.2 Please have a look at the mentioned pdf, to find the exact directory to paste the images!! Best regards, Wizard |
Follow us on