(0)| 1/14/2026 9:25 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hello, Perhaps the following links might help: Configuration of an HMI connection to S7-1500/S7-1200 CPUs and No connection to PLC after WinCC Panel Images V17 Update 6 What system messages, do you get on the panel? Do you have an Alarm View showing system messages? Best regards, Wizard |
| 1/19/2026 11:04 AM | |
|
Joined: 8/14/2020 Last visit: 1/19/2026 Posts: 458 Rating:
|
Hello racmatos If you want to view past system alarms, there are two options: a) Log system alarms to an alarm archive and display them from there in the alarm view https://support.industry.siemens.com/cs/us/en/view/109746939 b) Display system alarms from the alarm buffer Note regarding option b): On ComfortPanels, all alarms are automatically entered into the alarm buffer. When the alarm buffer is full, the oldest alarms are deleted. The alarm buffer therefore functions like a ring buffer (first in / first out). Therefore, it is advisable to check the system alarms immediately after the fault occurs. You can display the system alarms present in the alarm buffer as follows: Best regards, Costanza |
Follow us on