7/14/2008 12:18 PM | |
Joined: 10/18/2006 Last visit: 3/4/2022 Posts: 163 Rating: (3) |
Hi experts ! I´m having big trouble working with PCS7 v7.0. I´ve already worked some time witha project and had no problem at the beginning, but in the last days, i´m getting a strange error message when i try to open a CFC (and it doesn´t open). It doesn´t happen every time i open a CFC but randomly. Also a pop-up window is displayed, showing the message "the hierarchy folder couldn´t be read". Hasit ever happened to anyone? Thanks a lot in advance for your support. Best regards AttachmentERROR_SQL.zip (109 Downloads) |
7/14/2008 6:49 PM | |
Posts: 2661 Rating: (279) |
I have not encountered this but my guess is, your problem isrelated toWindows installation. I can see from your attachment that automatic Windows update is turned on. This is not good. You should not update your Windows with all patches. PCS7 is not tested with all patches. See the following FAQ: What should you watch out for when implementing Microsoft Security Patches in SIMATIC PCS 7? |
7/15/2008 11:43 AM | |
Joined: 10/18/2006 Last visit: 3/4/2022 Posts: 163 Rating: (3) |
Thanks for the tip ! |
8/12/2009 1:01 PM | |
Posts: 12 Rating: (0) |
Hi Experts. Reinitiating same problem ... I am using PCS7 V7.0 SP1 .... When exsiting project is opened there is no hierarchy folder in plantview visible. Can't open CFC chart, error popup comes with message "Cannot read hierarchy folder". Save as from simatic manager is also not works, unable to access AMDBase.db and AMDBase.log This project was running for month's without any problems. Please look at the attachments for more details Regards Nitesh
AttachmentErrors.zip (110 Downloads) |
Follow us on