Industry Online Support
Technical Forum
7/7/2006 10:22 AM | |
Posts: 38 Rating:
|
Hello Mighty Gurus, where can poor STEP5 beginner (=me) find some more detailed infos about diagnosing why the CPU falls into STOP? Thanks in advance Petr |
7/7/2006 11:35 AM | |
Joined: 4/24/2006 Last visit: 6/28/2024 Posts: 8698 Rating:
|
Hello, Mostly there is some information in the manual of the CPU, here's a link: http://support.automation.siemens.com/WW/view/en/1085940 See chapter 5.6 Best regards, Wizard |
7/7/2006 8:23 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
[quote user="peva"]where can poor STEP5 beginner (=me) find some more detailed infos about diagnosing why the CPU falls into STOP? Hello Peva, The Wizard have you given a link for a word-machine, there are also (the smaller CPUs) Byte- and WORD-BLOCK CPUs. [:o] For a Byte-CPU (for example the S5-115U CPU941...944) is the next link actual: S5-115U Programmable Controller it is also in chapter 5 described for the IStack, especially the Istack is not the same as for the CPU928. [:P] Also in the STEP 5 manual in Chapter 17 is the I- and Bstack described: SIMATIC STEP 5 V7.2 [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on