8/12/2009 8:54 AM | |
Joined: 7/27/2009 Last visit: 8/17/2009 Posts: 3 Rating: (0) |
Hi, I am just studying about the PLC. exactly about DB size. There are something I do not understand. As you can see the PDF file I attached, the upper part of the file, there are 4 kinds of CPU. The DB numberof the first two items(CPU 312, 314) are 511, and the others are 1023. However, the DB sizes are all same, 16Kbytes. here' s thing. the size(16Kbytes)meansone DB size? so, for example, CPU 312's DB total size is 8176Kbytes?. up to now,I don'tunderstand and think likethat. In my opinion,the size(16Kbytes) is the total DB size, so, just one DB size is about 31.3(16000/511) bytes.Am I right? please help me out of this problem. Thanks in advance for you helps. lotsof love. AttachmentDB size.pdf (953 Downloads) |
8/17/2009 7:08 AM | |
Joined: 7/27/2009 Last visit: 8/17/2009 Posts: 3 Rating: (0) |
Hi, Aret~! |
Follow us on