7/17/2009 10:43 PM | |
Posts: 2661 Rating: (279)
|
Without knowing the internals it is very difficult to guess the exact synchronization mechanism. But from the attached page in the manual it seems that the system program "keeps track" of the changes and synchronizes the data. I vaguely remember testing this with a S5-155H many many years ago but I cannot vouch for this... Regards PS: An interesting discussion that should be carried forward by all means. AttachmentSynchronization.pdf (268 Downloads) |
This contribution was helpful to2 thankful Users |
7/19/2009 2:54 AM | |
Posts: 2661 Rating: (279)
|
I agree. Smiffy, you should give this a try (see attachment). I used this scheme for comm between a 417H and 315-2DP (with 343-1) and it worked well. Yes, the synch modules with the FO link are primarily responsible for the data comparison. I doubt it... Regards AttachmentS7_Connections.pdf (267 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on