3/3/2007 7:58 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, There is a PROFInet handbook "Automating with PROFINET", Order No. A19100-L531-B906-X-7600. This is a nice book that describes very well the things you have to know about PROFInet. To get some information about the timing (this is for a PROFIBUS network) of the ET 200S station you may read: Isochrone Mode A presentation can be downloaded from: PROFINET IO UK Presentation at Coombe Abbey A device for Profinet is the CP 343-1CX10: Manual Part CP 343-1 Lean 6GK7343-1CX10-0XE0 Another handbook is also a good one: PROFINET System Description |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on