Industry Online Support
Technical Forum
9/14/2009 2:42 PM | |
Posts: 13 Rating: (1) |
I don't think I fully understand your problem. You mayrotate the workpiece plane from a part program or from operator settings: 1. From part program: Intoa new program or into MDA mode write ROT Axis=Value. For example, to rotate the frame 45 degrees around Z axis (so that axes X and Y are rotated) write ROT Z45 or ROT Z=45. To disable rotation write ROT (without any parameter). If you need a chain of rotations you may write ROTA instead of ROT (meening additive rotation). 2. From operator settings: Just go to "Parameters" Operating Area, Work Zero Offsets, select a work offset (e.g. G54) and there you may select a rotation. All you need after that is to call the work offset (e.g. G54). More about this in the "Programming manual Fundamentals", chapter 6. Frames. (additional examples with explanatory drawings). (http://www.automation.siemens.com/doconweb, select SINUMERIK and SIMODRIVE or SINUMERIK and SINAMICS, then USER, then this manual). You may read the .pdf file on-line or download so the operator / programmer of the machine may also read-it. Best regards, |
Follow us on