10/4/2009 8:25 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Waqas, Let's separate in two side. 1. Connecting the PLC; 2. Connecting the configuration computer; More info about ways and type of conections cables you could look at manual . Also look at Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?. I suggest you -MPI connection - use simple profibus cable, connectors plus necessaries setings in Microwin. OR - Ethernet - you need CF Ethernet card to extend the TP270 by an Ethernet interface (Tested network cards for OP/TP270 you will find under the Entry ID: 17888073 ) and CP243-1 in CPU side. Hope this will helps. best regards, Hristo Mihalev |
Follow us on