2/25/2009 1:29 PM | |
Posts: 4 Rating: (0) |
So, making sure that the USB converteris set as COM1 of COM2 port should solve the problem? The kind of USB converter, can this also be important? |
2/25/2009 2:07 PM | |
Joined: 4/24/2006 Last visit: 8/8/2024 Posts: 8713 Rating: (1166) |
Dear Kikof, Have you seen this faq: http://support.automation.siemens.com/WW/view/en/13904923 So the USB-RS232 convertor could be the problem Best regards, Wizard |
10/14/2009 6:54 PM | |
Joined: 12/20/2008 Last visit: 7/8/2024 Posts: 19 Rating: (0) |
Dear All, i have the same problem right now. Do you rember how the problem had been solved? Thx in advance
|
10/15/2009 9:04 AM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed inthese threads Problem downloading (--- PANEL OP 7 ---). Connect OP7 <-> PC(USB) via converter RS232<>USB. CANNOT DOWNLOAD PROGRAM FROM LAPTOP TO OP3. Simatic OP 27 and PC. Please continue to discuss in the last mentioned thread. Best regards O_Moderator |
Follow us on