Industry Online Support
Technical Forum
11/11/2009 10:43 AM | |
Posts: 18 Rating: (0) |
Hello, Ispossible to read program from S5 110 and wich sw and cable is needed? Thanks! |
11/12/2009 6:27 AM | |
Joined: 10/7/2005 Last visit: 10/31/2024 Posts: 3025 Rating: (1055)
|
Hello Dragc it is generally possible, but you didn't say which 110 you have. I hope for your sake that it is a 110S (last seen when Columbus discovered America) and NOT a 110A(last seen when the Pyramids where built). Anyway, please check your 110 part numberand below are some links for the 110A and 110S that will get you started: S5-110A PLC LADDER CHECKING ONLINE AG110A: on-line operation with more recent PGs No on-line connection to AG 110A, AG 130A/K How do you connect the PG the PLC S5 110S More can be found if you search the Siemens service & support web for S5-110A or S5-110S. I hope this helps and good luck |
Last edited by: fritz at: 11/12/2009 6:30 AMCheers |
|
This contribution was helpful to1 thankful Users |
Follow us on