11/13/2009 12:04 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Dear YogendraG, Are you using latest Servicepack and Hotfix? Here you can download Servicepack 1: Servicepack 1 for WinCC flexible 2008 And Hotfix 2: hotfix for WinCC flexible 2008 + sp1 Best regards, Wizard |
11/13/2009 1:56 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170) |
When does this problem appear? Directly after startup or every time you start the RT project? |
Have Fun! |
|
11/14/2009 11:56 AM | |
Joined: 11/9/2008 Last visit: 4/18/2024 Posts: 402 Rating: (6) |
Dear Wizard, Thanx for ur reply.Sorry i forgot to write my winccflex version it is Winccflex 2008 SP1 HF1. I got one solution. In connection if i change the state online to offline then it runtime works fine then again i switch to online thenit start to create problem. I don't understand this thing plz. help me. Regards, Yogendra G |
11/14/2009 11:57 AM | |
Joined: 11/9/2008 Last visit: 4/18/2024 Posts: 402 Rating: (6) |
Dear TomDeWou, When put my project in runtime. Regards, Yogendra G |
Follow us on