12/17/2009 5:44 AM | |
Joined: 4/23/2007 Last visit: 6/4/2024 Posts: 58 Rating:
|
I am using a SICK Laser transducer (DME5000) which has GSD file "sick069d.gsd" (attached). The module is constantly giving a diagnostic message "Module OK" (every 10ms) which is filling up the buffer and due to this I am not able to trace any other DP slave errors. I also checked out the GSD file as I thought the message is being defined in the GSD file but I could'nt find that message. I want to eliminate this message as it is sheer folly to have a message for healthy situations. Attachmentsick069d.zip (117 Downloads) |
"There is no spoon." |
|
Follow us on