12/29/2009 9:58 PM | |
Joined: 9/28/2005 Last visit: 5/23/2024 Posts: 2957 Rating: (242) |
Hello, You create multiproject as normal project, but just choose Multiproject tab. I mean "File ---> New ---> Multiproject tab" and everything else as in usual project. Now what do you mean about variable excange between projects ? If you mean to exchange data between two PLCs you still need to configure connections and use connection blocks as in usual project. Multiproject gives you an ability to work with two or more project as with one project and it is easier to configure connections in NetPro if you have all projects in one. For example if you want to make connection to PLC which is not in your project then you'll have problems in NetPro as you don't see other PLC there (you can use unspecified partner of course). So you create multiproject, insert your project here and also other project here and then if you go to NetPro you can see other PLC and configure connections easily. You can also find some useful info here and don't forget about Step-7 online help system. |
Last edited by: Darius at: 12/29/2009 10:00 PMBest regards, |
|
Follow us on