Industry Online Support
Technical Forum
1/7/2010 7:09 AM | |
Joined: 9/16/2008 Last visit: 4/2/2024 Posts: 56 Rating: (0) |
Hi, Wish All the members of Siemens Forum A Happy New Year 2010. I've a problem. I'm using S7Prof2006 R6 under Win XP SP3 and Win CCV6.2 SP2. I've craeted a project with S7 400. After inserting all the drives and encoders I've compiled and made the software. After completion of the Software while testing I found an error while compiling the hardware (the Log file attached). There is no Help text for those errors also. Can Nayone help me in this regard. My project has been completed and I want to test it with real CPU. Find attached the LOG file and Hardware screen shot. I'm working locally. Not from any other system. I've done Consistency Check but it has completed without any error. I've also all GSD file related to the devices. Regards AttachmentHardware Compilation.zip (107 Downloads) |
Follow us on